Two Primary Power Connector Classification by NEMA
In those environments where equipment needs to be powered on at all times for safety or productivity reasons, a twist-lock receptacle can be a lifesaver.
There are two primary classifications of power connectors as determined by the National Electrical Manufacturers Association (or NEMA), the governing body for power plugs and other receptacles used for AC electricity within the United States and other nations: straight-blade connectors and twist-locking connectors.
Straight-blade Connectors
A straight-blade connector, such as a standard three-prong wall outlet, requires that you simply insert or remove a plug to generate electricity to a machine or device. Modern outlets, also known as GFCI (ground fault circuit interrupter) receptacles, feature safety technology that effectively breaks the electrical circuit if it’s exposed to water or extreme heat. (There are also versions designed specifically for outdoor use.) But if you need the power to stay on, machines plugged into these simple outlets can easily become disconnected because of vibrations or human error.
Twist-locking Connectors
A twist-lock receptacle or socket incorporates another element of protection to lock a connector into place so it cannot easily become unplugged. To connect properly, the plug must be twisted, which makes it useful in hospitals with vital medical equipment or in offices or factories where computers or assembly lines need constant power. Twist-lock receptacles are available in both female and male versions and vary by other factors, including the amps, number of poles, number of wires, and NEMA ratings.
NEMA Alphanumeric Code
When working with connectors during a building design or renovation, you may encounter a NEMA alphanumeric code that indicates what outlets currently exist or are part of a new wiring system. The letters at the beginning of the identification code can help you easily determine the type: Those codes that begin with the letter “L” are curved blade and twist-locking; those without an “L” preceding the code’s numbers are always straight blade and non-locking.
How Twist-Lock Receptacles Work
Usually, the male connector on a twist-lock receptacle features curved prongs that plug into the outlet and are twisted to lock them into place. To minimize the chances of it being unintentionally disconnected, the plug must be turned the opposite direction to be unplugged. Unless this process is followed, the plug for the electrical device or machine will stay inserted into the socket and electricity will continue to flow.
It is important to point out that twist-lock receptacles should not be seen as a viable solution for disconnections that might occur because the plug in question is located in an area with heavy foot traffic. Tripping over an errant cord can still occur even with the installation of a twist-lock receptacle, and this can create a dangerous situation if the cord is stretched or frayed to expose wires with live electrical current.
In the cases where a cord is simply in the way of employees or passers-by, the outlet should be reconfigured within the layout or at the very least secured safely to the ground to minimize any potential safety hazards.
Wiring a Twist-Lock Plug
To install a twist-lock receptacle, you need to work with the plug’s three color-coded wire terminals: a positive terminal, a neutral terminal, and a ground terminal. Here are step-by-step instructions:
- Step 1 - Wrap the “hot” or positive wire (typically it is the black wire) in a clockwise direction around the screw found in the gold terminal and then secure the screw tightly.
- Step 2 - Take the neutral wire, which is oftentimes gray or white, and wrap it clockwise around the screw in the silver terminal in the twist-lock plug. Make sure the screw is tight.
- Step 3 - Find the ground wire (it should be green or green and yellow) and twist the wire’s strands to create one thread. Take that thread of wire and wrap it around the screw in the plug’s green terminal. Tighten the screw.
Adapters
In some situations, such as when working with stage lighting, certain adapters are necessary when there are a variety of power connection systems available. One of the most common is an adapter that facilitates the connection between an Edison, also known as a “house” or common household plug, with a twist-lock outlet.
By design, Edison plugs feature two flat prong blades and a semi-round ground pin. But there are variations depending on the amps of a specific plug. For example, a 20-amp rated plug usually has one blade perpendicular to the other. A 15-amp plug typically has two parallel blades. When purchasing adapters, be sure to check the amp levels and corresponding blades to make the desired connections.
Product Compliance and Suitability
The product statements contained in this guide are intended for general informational purposes only. Such product statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand and follow all manufacturer instructions.