Visit here before you buy! We’ve researched, compared, and compiled the data on tons of products so you don’t have to.
Cylindrical locksets are the type of locks found on doors in most commercial buildings. They’re inexpensive, easy to install and replace, and can conveniently be rekeyed. However, selecting the proper lockset function can sometimes be confusing, especially when faced with so many options.
Oil burner nozzles come in various spray angles and spray rates which determine the efficiency of an oil burner.
Waterless urinals are designed to work in areas where pressurized water isn't available or water restrictions prevent the use of a standard flush valve urinal.
A solenoid valve is a motorized valve and most frequently is used to control the flow in a pressurized liquid, gas, or air system. They often have a variety of operations within a system, including switching on/off, releasing, dosing, distributing, or mixing fluids.
The answer to the question of how to select the right drill bit begins with the material you will be drilling. Another key consideration is the purpose of the hole you need to create.
Selecting the proper style and size pump for a submersible pumping application doesn’t need to be a daunting task!
There are lots of different applications for air compressors, so how do you choose the right air compressor for the job? A little understanding of air compressor basics should help in finding the right tool for the job.
A safety storage cabinet is one of the most important items you can use if you have to store flammable, corrosive, or combustible liquids.
While it may be simplistic to think of a fire extinguisher as "just" a fire extinguisher, the National Fire Protection Association (NFPA) actually classifies fires, and fire extinguishers used to fight them, into five general categories.
With so many home cooling systems on the market, it can be a challenge to decide what type of unit is worth getting. If you simply want to move warm internal air out of the entire house and replace it with fresh air from outside, a whole house fan may be what you’re looking for.
From the type of valve to the mounting style, commercial toilet parts vary in many ways from a residential toilet. When installing a new toilet and flush valve, be sure to check local codes for selecting the correct items for installation and GPF (gallons per flush) compliance in your area.
Condensate pumps are used to pump condensate, or water, produced from HVAC, refrigeration, condensing boiler, furnace, or steam systems.
Designed to circulate in fresh air while removing stagnant, fume-laden or stale air within a confined space, exhaust fans are available in a variety of types and sizes.
Cam locks are a type of hardware that offers a simple locking solution, especially popular for use with office furniture such as desk drawers and filing cabinets. These locks secure items that require stowing, and can restrict access for anyone not having a key.
Time delay relays control the flow of electrical power and can be used to control power to many different types of electrical loads. Combining electromechanical output relay capability with control circuitry, these relays are pre-engineered to perform up to eleven time delay functions.
When it comes time to consider proper filtration for any HVAC system, a few things to keep in mind include the correct filter size, filter material, filter type, the environmental conditions the filter is used in, and MERV ratings.