Determining what size pipes you need for your project can be confusing. Many people assume pipe size is the outer diameter of the pipe—but “pipe size” actually refers to what is called “nominal diameter.”
Fittings can be just as confusing. Their inside diameters must be large enough to fit over the pipe's outside diameter. A half-inch plastic elbow, for example, has an outside diameter of about 1-1/4 inches.
Use this guide to help you find the pipe and fitting sizes you need for your next project.
How To Measure Pipes and Tubes
Convert Actual Diameter to Nominal Diameter
The easiest way to find what nominal pipe size you need is to use follow these steps and use the conversion chart below.
For Male Threads1. Measure the Outside Diameter (OD) of your pipe or pipe fitting:
2. Use the chart on this page to find the nominal diameter (pipe size). |
![]() |
For Female Threads1. Measure the Inside Diameter (ID) of your pipe or pipe fitting (use a ruler or tape measure). 2. Use the chart on this page to find the nominal diameter (pipe size). |
![]() |
Nominal Diameter Conversion Chart
(All Measurements in Inches)
Outside or Inside Diameter | Decimal Equivalent | Nominal Diameter | Typical Threads Per Inch |
5/16 | 0.313 | 1/16 | 27 |
13/32 | 0.405 | 1/8 | 27 |
35/64 |
0.540 |
1/4 | 18 |
43/64 | 0.675 | 3/8 | 18 |
27/32 | 0.840 | 1/2 | 14 |
1-3/64 | 1.050 | 3/4 | 14 |
1-5/16 | 1.315 | 1 | 11-1/2 |
1-21/32 |
1.660 | 1-1/4 | 11-1/2 |
1-29/32 | 1.900 | 1-1/2 | 11-1/2 |
2-3/8 | 2.375 | 2 | 11-1/2 |
2-7/8 | 2.875 | 2-1/2 | 8 |
3-1/2 | 3.500 | 3 | 8 |
4 | 4.000 | 3-1/2 | 8 |
4-1/2 | 4.500 | 4 | 8 |
Pipes vs. Tubing
Pipes vs. Tubing
Pipe and tubing are not measured the same way. Tubing is measured and named based on the actual outside diameter of the tube.
PEX, or Cross-Linked Polyethylene Tubing, is another technology fast becoming popular, and it is measured and named by inside diameter.
Example:
Pipe vs. Tubing |
Outside Diameter |
1/2” size pipe | 27/32” |
1/2” size tubing | 1/2” |
Select Thread Type
One of the most common thread types is National Pipe Thread (NPT). These come in male (NPT, MPT, or MNPT) and female (FPT or FNPT). These are usually tapered threads used in joining and sealing pipes.
Another common thread is National Standard Free-Fitting Straight Mechanical Pipe Thread (NPSM). These straight thread pipes are typically used for mechanical joints.
BSP thread form stands for British Standard Pipe. It is based on trade size rather than actual diameter.
Product Compliance and Suitability
The product statements contained in this guide are intended for general informational purposes only. Such product statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand and follow all manufacturer instructions.